Sensata Internet of Things (IoT) Solutions

Sensata Internet of Things(IoT) Solutions include an expansive range of components that provide accuracy, reliability, and durability combined with the convenience of wireless connectivity and enhanced security. The robust portfolio of wireless systems simplifies and lowers the cost of connecting data from assets in hard-to-maintain locations for smart factory solutions. The breadth and configurability of Sensata’s wireless system devices, which include wireless pressure and temperature sensors, receivers, transmitters, and gateways, simplify the addition of IoT connectivity for industrial equipment providing tangible benefits to the overall operation.

Features

  • Reduced operational costs - Through wireless connectivity solutions, the complex process of producing products can be simplified to its most basic components. Wireless solutions enhance automation systems to be continuously as efficient as possible: generating little waste heat, using the minimum power, and efficiently using all plant resources. Wireless solutions can also eliminate the need for work by electricians as the solutions work on low voltage. All this makes manufacturing more cost-efficient and productive.
  • Increased labor productivity - End-to-end factory automation can double or even triple production compared to plants that use only a few automation systems. Manufacturing equipment incorporating wireless connectivity can often be kept running for extended periods. Eliminating route-based maintenance and other manual tasks may positively impact manufacturing and maintenance resources.
  • High machine asset availability - In a company with machines that have little availability and low production times, users will have less time and opportunities for high performance and quality. Wireless connectivity enables high availability and means less downtime and more throughput. When machines are running and being used, profitability increases.
  • Increased reliability - When there is an increase in a plant's reliability, there will be an increase in production and company profit. A company can eliminate long and complex wiring home runs, pinched and cut cables, and the associated material and labor costs to replace them by implementing wireless connectivity.
  • Optimized performance - Manufacturing optimization is the practice of using data to build better products faster, intending to be more competitive. Implementing wireless sensors and systems in the automation equipment allows close control of manufacturing variables. The system brings the data to the right people at the right time and place. When processes change state, the right action can be taken. This quick response helps maintain operations and performance.

Videos

Published: 2022-11-08 | Updated: 2023-03-21