Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

Infineon ICL5101 Resonant Controller IC with 650V High-Side Driver Now at Mouser

April 13, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now stocking the ICL5101 LED Resonant Controller IC from Infineon Technologies. Integrating a half-bridge controller with a Power Factor Correction (PFC) stage in a single package, the ICL5101 extends Infineon's existing portfolio of lighting control ICs to address lighting systems in the range of 40Watts to 300Watts. The high level of integration ensures a low count of external components, enabling small form factor designs that are ideal for compact power supplies in lighting applications such as an LED driver.

The Infineon ICL5101 LED Resonant Controller IC, available from Mouser Electronics, includes both a half-bridge controller and a PFC stage. The PFC stage operates in CrCM and DCM mode, allowing LED lighting to be dimmed from 100 percent down to an extremely low 0.1 percent of its nominal power load without audible noise. The half-bridge resonant stage provides high- and low-side gate drive functionality for discrete MOSFETs rated up to 650V, and features a self-adaptive dead time control of the half-bridge driver from 500ns to 1.0µs. Other features of the resonant half bridge controller include improved operation control in magnetic saturation during start-up, and advanced error detection.

The Infineon ICL5101 LED Resonant Controller provides an ultra-fast time-to-light of less than 200ms under any conditions, and a high efficiency of up to 94 percent. The device is extremely stable over line voltage variations, and is equipped with a comprehensive set of protection features including external over temperature protection, overload protection, short circuit protection, and capacitive load protection to increase system safety. All operation parameters of the IC, including protection features, are adjustable by using external resistors, making this chip an ideal choice for reliable systems that are easy to design by using approximately 25 percent fewer components compared to similar solutions which require separate PFC and resonant ICs.

The ICL5101 LED Resonant Controller supports outdoor use by an extended junction temperature ranging from -40°C to 125°C, and is available through Mouser Electronics in a compact, PG-DSO-16-pin package. The device is targeted toward a variety of lighting applications, including Indoor/outdoor high-power LED lighting; high-bay/low-bay lighting; street lighting; parking garages and area lighting; and office/shop lighting.

To learn more, visit:
http://www.mouser.com/new/Infineon-Technologies/infineon-icl5101-controller/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About Infineon Technologies
Infineon Technologies is a leading global designer, manufacturer and supplier of a broad range of semiconductors used in various microelectronic applications. Infineon's product portfolio consists of logic products, including digital, mixed-signal, and analog integrated circuits, as well as discrete semiconductor products.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room