Mouser Now Stocking onsemi NCN26010 Ethernet Controller, Providing Reduced Wiring and Costs

New Product Announcement

Connect With Us


June 5, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the NCN26010 Industrial Ethernet Controller from onsemi. This 10BASE-T1S Ethernet controller is designed to provide reliable multi-point communication in industrial settings.

The onsemi NCN26010 is a 10Mb/s, IEEE 802.3cg compliant device including a media access controller (MAC), a PLCA reconciliation sublayer (RS), and a 10BASE-T1S PHY, designed for industrial multi-drop Ethernet networks. The device can enable more than 40 nodes on a single twisted pair, exceeding five times the amount of nodes requested by the IEEE 802.3cg standard, reducing installation cost and set-up complexity. This PHY + MAC controller for 10BASE-T1S can connect to controllers, sensors and other devices without the need for an external MAC.

The NCN26010 reduces in-cabinet wiring up to 70% while significantly increasing bandwidth. In backplanes, it simplifies the layout and power distribution without impacting data rates or latencies. Many applications, such as elevators, will be able to increase data throughput over existing wiring with the device and, due to the ability to carry power over data cables, complex sensor networks can be built upon simple and low-cost cable runs.

The NCN26010 makes an ideal replacement for legacy point-to-point and multi-point industrial communication standards. The T1S MAC/PHY device can replace RS-485, CAN, RS-232, HART and others. As a result, greater data throughput is achieved over existing wiring, eliminating the need to re-pull wires which is often the greatest expense in a networking installation. The NCN26010 also features a proprietary enhanced noise immunity feature which is essential for installations in electrically noisy industrial environments.

The NCN26010 controller is supported by the NCN26010XMNEVB 10BASE-T1S MACPHY evaluation board, the NCN26010BMNEVB Adapter Board, and the NCN26010XMNEVK 10BASE-T1S SPE evaluation kit, all available from Mouser.

To learn more about the onsemi NCN26010 Industrial Ethernet Controller, visit https://www.mouser.com/new/onsemi/onsemi-ncn26010/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About onsemi

2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764