A Worthy Upgrade
Improved Tone with Just a Little Time, Money
By Will Kelly, Vintage Guitar® magazine
You are living in the golden age of guitar accessories. Every piece of guitar hardware has been
thoroughly studied, analyzed, "improved" and marketed, and it can be a challenge wading through the hype
to figure out what works (and helps), and what doesn't. Through my years of application and experience, I've come to
recognize a couple of can't-miss upgrades that are worth the money, time and effort to implement.
I'm a huge advocate of quality electronic components. The majority of players who want to improve their guitars
usually start by upgrading electronic components. These are usually easy to accomplish, mostly reversible mods that
bring quick and tangible results. In my opinion, there is no better upgrade to a budget or mid-priced instrument
than installing professional-grade switches, pots and jacks. These things do make a difference in tone as
serviceability.
-
Bourns is an
American company that makes cool potentiometers. Those I use most are the Model 82 Vintage units, which are sealed,
permanently lubricated and do not use carbon tracks to provide variable resistance. Rather, they have conductive
plastic resistance tracks that do not wear out. They are noiseless and transparent-sounding. They do require
different installation techniques, the major difference being in how they're grounded.
-
For grounding connection, Bourns supplies a special metal compression washer with a lug tab. The threaded metal
casing of the post does make great ground connections when used with metal mounting arrangements, such as an
amplifier chassis, but the guitar modder will have to use this washer to ensure proper grounding. To install the
Bourns on a typical Strat-style guitar, snap a quick picture of the
wiring connections and label the wires with small pieces of masking tape. Then you can snip the wires from the
terminals and ground casing, and remove the pots.
-
If you have a guitar with mini pots, you'll probably find the Volume and tone control holes in the pickguard
aren't large enough for a Bourns. Use a drill with a 3/8" bit to enlarge the hole to correct diameter.
Install the Bourns with the special washer in place between the pickguard and the body of the control pot. In
this instance we're replacing the master Volume pot, so I chose a 250k audio-taper control, which is the stock
spec for this style of instrument.
-
The terminals are in different positions than a traditional potentiometer, but there are still three and they
perform the same function. On a master Volume control in a passive instrument, the end terminal is usually
grounded so the audio can be rolled off. With Bourns pots, you'll have to solder a wire that connects to the
grounding washer rather than simply bending the terminal lug and soldering it to a metal case. The other two
terminals are wired in the traditional manner, with the input going in the end terminal, and the output coming
out of the center lug.
-
I solder a small-valve treble-bypass capacitor
between the input and output terminals of a Volumen control, to bleed treble back into the signal as the control
is turned down. However, I've found that I don't need to use additional resistor to adjust the taper of the pot,
like I had to do with the carbon-track pots. The Bourns have an
incredible consistent taper and smooth operation with no "play" or looseness.
Tone controls in a Strat-style guitar are wired differently than Volume controls; the end-terminal lug is
usually shunted to ground with a small capacitor. This provides carrying degrees of treble roll-off depending on
the value of the capacitor. Most Strat-style, single-coil instruments use a .047-uF capacitor as a good match
for the brighter-sounding single-coil transducers. Humbucker guitars more typically use .02-uF capacitors o
better handle the thicker tone. Replacing these is basically the same as the Volume control.
-
The shafts are configured with the standard splined/split ends that fit most plastic push-on knobs. Once the
Bourns are installed, there's no aesthetic difference compared to the old setup. These controls are a great bang
for the buck because they have a long maintenance-free life. The average guitar player will simply never wear
them out. They sound transparent and have a great feel. They do cost a little more than traditional pots.
If you're unsure about the soldering and wiring, take the instrument to a pro repair shop. They'll be more than
glad to install them for a reasonable bench charge. This is definitely one upgrade that's worth your money, time and
effort.
Will Kelly is a guitarist, engineer, repairman, and collector who loves low-budget gear. His shop, Hard Knocks
Guitar, in Cary, North Carolina, has played host to countless instruments and amplifiers.